Virtual trade show | Machine tool

Where are you on the path to sustainability?
Take the next step: discover new solutions
for greater 
productivity starting with the first part

Control your robot with the TNC control

Cancel

live

Speak to your robot in KLARTEXT

Automated machine tools with a pallet system and a machine-tending robot have become an essential capital asset on shop floors. But the robot and machine tool are separate systems requiring different programming languages and often two experts familiar with them. Until now!

HEIDENHAIN has found a way to make robots understand Klartext. Users of HEIDENHAIN TNC controls can program machine-tending robots from within the TNC user interface by teaching-in the desired movements and saving them as Klartext code in the NC program. This saves time and enables more versatile automation during machine setup. Find out more in our video.

Cancel

live

New hardware variants of the TNC

The TNC7 portfolio has the perfect hardware variant for every application, offering convenient touch operation on a 16-inch, 19-inch or 24-inch Full HD monitor. You can also choose between a full-sized keyboard unit or a compact machine operating panel. Regardless of the hardware, your productivity still goes up thanks to typical TNC7 features such as intuitive, context-sensitive user guidance and innovative software options such as MAS graphical 6D setup support, DCM dynamic collision monitoring and OCM high-performance trochoidal milling.

TNC7 basic: the 3+2-axis control 

The TNC7 basic lies near the lower end of the HMI portfolio, replacing the popular TNC 620. Its 16-inch touchscreen features Full HD resolution. Particularly space-conscious users can opt for a machine operating panel with only the most essential functions. The TNC7 basic can be used with the typical, wide-ranging TNC7 software options that boost user-friendliness, efficiency and process reliability.

Cancel

live
New
Cancel

live

The OC 310 multi-functional override controller

Two potentiometers in one multi-functional operating element: the new OC 310 override controller facilitates working with a TNC7, since the user can now regulate both the feed rate and rapid traverse with just this one operating element. The user is supported by the new “Conditional stop” software function, for intuitive, convenient and one-handed proving-out of NC programs. The user simply defines breakpoints in the NC program at which the control will stop during program run (such as before a tilting function, when the tool is changed, or when the machining feed rate changes to rapid traverse). The override controller vibrates to generate tactile feedback, simplifying the user's workday. Each user can define the events for which this function is active.

Manufacture with process reliability, use resources efficiently
HEIDENHAIN reduces your TCO and carbon footprint

New solution for your tools: VT 122
3-in-1 measuring camera

Combining three roles in one intelligent system, the new VT 122 vision system, in conjunction with the VTC software, handles the roles of tool presetter, tool microscope and visual inspector. Obtained straight from the machine’s work envelope, its images enable detailed inspection of the tool’s cutting edge and deliver the information needed for holistic tool evaluation. The system’s smart camera and software can automatically measure a tool’s length, diameter and wear width. Tools can be inspected without a trip to the metrology lab, allowing users to work faster while providing automated tool-wear documentation.

Cancel

live

The retrofit that improves process reliability

Detect tool breakage while avoiding knock-on damage and scrap. The TD 110 tool breakage detector from HEIDENHAIN accomplishes all of this from within the machine envelope and integrates seamlessly into automated processes. The TD 110 also saves time, performing breakage inspection up to six seconds faster per tool change.

Do you know about our encoders with added value for automation and robotics?
Discover the ECI 123 Splus with integrated vibration evaluation and the dual encoders for advanced robotics!

The Digital Shop Floor from HEIDENHAIN
Software, consultation and services for a 360° view of your shop floor

Cancel

live

New features for StateMonitor:
Energy monitoring and ERP interfacing

Collect, evaluate and visualize machine data with StateMonitor, the machine data collection software from the HEIDENHAIN Digital Shop Floor. StateMonitor gives you real-time insight into the production statuses of your CNC machines. The new version of the software includes even more innovative solutions: An energy monitoring feature analyzes detailed data about your machine’s power, compressed-air and process-water consumption, allowing you to identify optimization potential. And a new ERP interfacing feature ensures automatic data sharing with higher-level ERP and MES systems, thereby enhancing your operational visibility.

TNC Club Lounge

Do you use a HEIDENHAIN control? If yes, then you'll benefit from a visit to the TNC Club Lounge! It's a great place to swap ideas with other experts, learn about interesting and exclusive training opportunities, and network with your peers.

We'll show you how easy it is to achieve fast and perfect results with the intuitive operation and task-focused functions of the new compact TNC7 basic for 3+2-axis machines.

We'll share insights about how you can use your manufacturing resources more efficiently. You can also check out the new VT 122 measuring camera and the new energy monitoring feature of the StateMonitor software.

So take a moment to relax at the TNC Club Lounge and enjoy a cup of barista-brewed coffee!

For a fast overview: our video library

Cancel

live
Cancel

live

Playlist

Autoplay
    Cancel

    live

    Playlist

    Autoplay

      Even more technologies and innovative solutions for machine tools

      Five-axis machining

      TNC controls from HEIDENHAIN make 5-axis machining operations easy and reliable. Discover the advantages.
      Find out more

      Grinding with the TNC

      From roughing to perfect finishes in a single setup: not a problem with the TNC functions for jig grinding from HEIDENHAIN.
      Find out more

      Gen 3 drives

      Gen3 drives from HEIDENHAIN with state-of-the-art interface technology, improved specs and enhanced controller performance.
      Find out more

      HEIDENHAIN, an umati partner

      StateMonitor supports many interfaces. Naturally including umati, the universal machine-tool interface.
      Find out more